Blog
What is a sensor, how does it work, and what are the various types of sensors?
Sensors work by detecting physical changes in the device’s environment and output them as analogue voltages or digital signals. This is then sent to a human-readable display where it can be monitore...
Types of circuit breakers and their importance
As beneficial electricity is to our sustenance, unless it is dealt with proper precautionary measures, electricity can pose a serious threat to expensive devices, as well as to our loved ones. So, to ...
What are Variable Speed Drives? The Ultimate Guide
A variable speed drive is an electronic device used in electrical and mechanical driving systems which allows the user to conveniently control the AC motor speed. It is also helpful for monitoring the...
Everything to Know About Your Digital Meter
One of the best products among the latest developments in electronic technology is a device known as the digital meter. The reason why they are nicknamed "smart meters" or "advanced meters", is that t...
What is a thermal overload relay?
Thermal overload relays are designed to provide electromechanical protection to motors against overloading from drawing excessive input currents from the main circuit. These electronic components can ...