MCB

MCBs are electrical switches that are used for protecting low voltage circuits from damage caused by overload or short circuit. MCBs replace the fuse as an automatic means of removing power from a faulty system. During short circuit conditions, the sudden rise of current will cause an electromechanical displacement of the plunger associated with tripping coil or solenoid of the MCB. Typically, these circuit protection devices are rated for current loads up to 125A.

MCBs are very simple to operate, and also provide manual opening and closing of the circuit. You can determine the condition of a Schneider Electric MCB by observing the positions of the switching latch, whether it is closed, tripped or manually switched off. Our MCBs have three positions – on, off, and tripped – which makes it easy and safe for users and electrical service personnel to operate these devices. Schneider Electric MCBs have a very robust, maintenance-free construction that makes them ideal for home and commercial use. Our MCB frames are modular by design and easily fit in any modular MCB box. The rigid and strong housing is insulated and can be easily used in conjunction with other mounted components. Now you can check Schneider Electric MCB price online and place orders directly from our E-shop.

 
X
 
X
 
X
 
X
Hello World!